Behind the Rainscreen Facade: Are You Making One of the Most Common Subframing Design Mistakes?
The same panel loads can produce very different demands on the rainscreen subframing system. Why architects should verify how panel connections transfer those loads before accepting a subframing design.

The same panel loads can produce very different demands on the rainscreen subframing system. Why architects should verify how panel connections transfer those loads before accepting a subframing design.
One of the most common subframing design mistakes I encounter in rainscreen façades is assuming uniformly distributed loading on the rails without verifying that it represents how the selected panel connections transfer their loads. The total panel load may be correct even when the assumed distribution misrepresents the demands on individual rails, brackets, and anchors.
Two rainscreen façade proposals show the same panel dimensions, weight, wind pressure, and similar bracket spacing. One costs considerably less. Before deciding which offers better value, ask: Does the proposal reflect how the selected panel connections actually transfer loads into the subframing?
That difference can begin with a connection detail: which panel clips or connectors carry the panel’s weight, which transfer wind, and which permit movement. A support layout can look coordinated before anyone has confirmed that the panel supplier and subframing designer are working from the same assumptions.
For architects and façade consultants, making the attachment strategy explicit allows the team to compare proposals on a sound basis and resolve differences before they become procurement decisions or field problems.
Start with the panel connection
For U.S. projects, establish design loads under the adopted building code and its referenced edition of ASCE/SEI 7, Minimum Design Loads and Associated Criteria for Buildings and Other Structures. These requirements establish what the façade must resist. The load path describes how those forces reach the supporting structure.
In the two-layer subframing system illustrated in Figure 1, the sequence runs from panel clips into secondary horizontal rails, through primary rails and wall brackets, and into the anchorage and supporting wall. Every connection along that path must be designed for the forces it receives.
Figure 1. The Rainscreen Load Path
The panel material alone does not establish that sequence or the function of each attachment. Fiber cement, metal, aluminum composite material, and stone can use different fixing systems. Manufacturer guidance for certain concealed systems, for example, assigns gravity support and wind restraint to two upper hangers, while the remaining hangers transfer wind and permit specified movement. One upper hanger also serves as the panel’s horizontal fixed point, restraining horizontal movement at that connection. These are system-specific functions, not rules that can be inferred from the material name.
Movement is part of the same design decision. Sliding connections transfer wind acting perpendicular to the façade while permitting specified vertical or horizontal movement in the plane of the façade. The design must distinguish between panel expansion, rail expansion, and relative building movement, such as interstory drift or floor-edge deflection. Connections and joints must accommodate the required movement while maintaining gravity support and wind restraint. A vertical sliding clip alone does not resolve the assembly’s complete movement requirements.
A panel’s attachment strategy determines where its weight enters the subframing. Figure 2 contrasts two illustrative attachment models. Case A assumes that 15 clips share the gravity load equally. Case B assigns the panel’s weight to two designated upper gravity-bearing clips, while lower sliding clips transfer wind and permit vertical movement. Both models resist wind. They deliver gravity into the subframing at different locations. Gravity support, horizontal restraint, and permitted movement must follow the selected fixing system.
Figure 2. Gravity Support and Movement Connections
The total load stays the same while local demand changes
An attachment reaction is the force transferred at an individual panel connection. Consider a panel measuring 4 feet by 10 feet, with a self-weight of 8 pounds per square foot. Its total weight is 320 pounds of force, or 320 lbf. A uniform wind pressure of 30 pounds per square foot produces a total wind force of 1,200 lbf over the same panel.
For the six-attachment wind model in Figure 3, assign tributary heights of 3, 4, and 3 feet to three rows, with two attachments per row. A tributary height is the portion of the panel height assigned to that row in this simplified calculation. Dividing each row’s wind force equally between its two attachments gives the following comparison.
Load and assumed sharing | Total Panel Force | Force per attachment |
|---|---|---|
Gravity shared equally by 15 clips | 320 lbf | 21.3 lbf |
Gravity shared equally by 2 upper supports | 320 lbf | 160 lbf |
Wind shared equally by 15 clips | 1,200 lbf | 80 lbf |
Wind assigned to 3 rows with 2 clips per row and tributary heights of 3, 4, and 3 ft | 1,200 lbf | Top row: 180 lbf Middle row: 240 lbf Bottom row: 180 lbf |
The panel has not become larger or heavier. Assigning its weight to two upper supports produces a gravity reaction of 160 lbf at each support, 7.5 times the 21.3 lbf equal-share value in the 15-point model. For wind, the six-attachment model’s middle-row reaction of 240 lbf is three times the 80 lbf equal-share value.
These simplified load allocations illustrate the effect of the assumed attachment strategy; they do not establish the reactions or capacity of a particular assembly. Equal load sharing must be supported by the selected system’s behavior, rather than inferred from the number of attachments.
Figure 3. Same Panel Loads, Different Connection Reactions
The distinction is between attachment reaction models. Fifteen equal clip forces remain discrete forces. Replacing those forces with a uniformly distributed load on a rail is a further modeling idealization whose suitability must be checked. Uniform wind pressure on the panel does not establish uniform loading of the rails or equal demand at their connections.
These clip or connector reactions are the starting loads for the subframing analysis. Rail spans, support locations, continuity, stiffness, and connection behavior determine how those inputs reach the primary rails, brackets, anchors, and supporting structure. A connection designed for Case A’s assumed reaction may require different fastener sizes, quantities, or details when Case B applies. The ratio between clip forces should not be applied unchanged to every downstream fastener or anchor.
Even when two layouts contain the same number of secondary rails, different clip forces and connection locations can produce substantially different demands on those rails and their connections.
Reconcile the attachment strategy before procurement
The attachment strategy may still be unresolved when the subframing is priced, engineered, or even ordered. Early pricing may reasonably require assumptions. The risk is allowing those assumptions to remain in the design after the selected panel system has established a different load path.
A panel supplier can develop a fixing scheme while the subframing designer analyzes a different support arrangement. Both sets of drawings can reach the installer before anyone reconciles the load paths. Each participant may have made a reasonable decision within their scope, yet the complete assembly remains uncoordinated.
The panel shop drawings, subframing calculations, and installation details should reflect the same attachment strategy, connection locations, load-transfer functions, and movement provisions. Receiving two drawing sets does not establish that they describe one coordinated assembly.
The subframing structural submittal should document the load path and identify the panel drawing revision used as the design basis. Clear references between the documents should allow reviewers to trace the panel attachment reactions through the subframing calculations to the connections shown in the installation details. The design assumptions must be traceable to the assembly being built.
After procurement, reconciliation can mean revised brackets, changed anchorage, additional engineering, or field modifications. Before release, the same discussion gives the team an opportunity to select an efficient arrangement. It also improves bid comparisons. A lower price may reflect a better solution; it may also reflect a different assumption about where the loads enter the supporting system. The proposal should make that distinction reviewable.
Where the loads enter changes the subframing design
The panel’s total weight and wind force remain the same, but its attachment strategy determines where those forces enter the subframing. The rails then distribute these inputs to the wall brackets and anchorage. Two configurations with the same number of rails and brackets can therefore place substantially different demands on those components.
Figure 4 contrasts two ways of introducing the same panel loads into the subframing. In the distributed-load idealization, loads are spread along the secondary horizontal rails. In the discrete clip arrangement, forces enter at specific clip locations on the outer support lines. Although no panel clips align with the central primary rail, the horizontal rails can still transfer load to it. Rail spans, continuity, stiffness, support locations, and connection behavior determine the resulting demands on each primary rail, wall bracket, and anchor.
Assuming uniformly distributed rail loading without checking the selected attachment strategy can underestimate demand at the connections receiving concentrated inputs. More rails and brackets do not, by themselves, establish adequate support where the largest forces occur. The design must trace those forces through the subframing and establish the demand on each rail, bracket, anchor, and fastener.
Figure 4. How Panel Connections Shape Subframing Demands
A rail without an aligned panel clip is not automatically unnecessary. It may receive loads through the horizontal rails, support an adjacent panel, or serve another required function. Confirm its role before changing the layout.
The thermal consequence also depends on the assembly. Unnecessary supports that cross the insulation can introduce additional heat-flow paths. Attachment material, geometry, continuity, and spacing influence effective wall performance. A secondary rail located entirely outside the insulation should not automatically be treated as another insulation-crossing thermal bridge.
This is the Performance Knot in practice: structural performance, thermal performance, and constructability must be coordinated. A structural change can alter attachment density, thermal bridging, installation sequence, or the ability to verify the work. A conservative choice in one area can impose costs elsewhere without resolving a mistaken assumption about the load path. The objective is an assembly whose required performance has been checked across all three strands.
Make the coordinated design basis visible
Architects and façade consultants can turn this coordination problem into a specific submittal requirement. Request one coordinated load-path exhibit that connects the panel shop drawings, subframing calculations, and installation details. It should identify:
The selected panel and fixing system, including the drawing revision used for design.
The attachment locations and the connections that carry gravity, resist wind, or permit movement in specified directions.
The panel attachment reactions used as inputs to the subframing calculations and the analysis that carries those forces into the supporting structure.
The provisions for panel, subframing, and building movement, together with the installation details and field checks that verify the intended behavior.
Reviewers should be able to follow an attachment on the panel drawing into the calculation model and then locate the corresponding connection in the installation details. Crews and inspectors should be able to identify the intended clip types, restraint locations, and movement clearances.
Figure 5. Coordinating Drawings, Calculations, and Installation
Reconcile discrepancies before the affected components are released for procurement or fabrication. When a substitution changes the fixing system, support arrangement, or movement strategy, revisit the affected structural, thermal, and installation requirements. Change one. Recheck all three.
Confirm the strategy for every panel selection
The same coordination must follow every panel selection and substitution. Fiber cement, terracotta, aluminum composite material (ACM), ultra-high-performance concrete (UHPC), metal, and stone can use different attachment strategies. Even within one material category, connector locations, gravity supports, wind restraints, and permitted movement can differ. Figure 6 illustrates this range. A material name or a familiar support layout cannot establish how the selected assembly behaves. The schematics illustrate fixing principles rather than installation details.
Frequently Asked Questions
Does uniform wind pressure justify uniform loading on every rail?
Uniform pressure acts on the panel. Its connections deliver forces to the rails at specific locations. A uniformly distributed rail-load model is appropriate only when the designer has verified that it adequately represents those inputs for the checks being performed.
Can a sliding connection resist wind while allowing movement?
Yes. A sliding connection can resist wind perpendicular to the façade while allowing specified movement in its plane. The detail must identify the permitted directions and available travel.
Is a primary rail unnecessary when no panel clip aligns with it?
It may still receive load through horizontal rails or support adjacent panels. Verify its role in the complete load path before removing it. It may be there to keep the layout consistent as adjacent panels may need it.
Verify the load path before accepting the layout
Before accepting a support layout or comparing its price, confirm that the selected panel connections, calculated reactions, and movement provisions describe the same assembly across the drawings and calculations. The forces leaving the panel must be the forces its supports were designed to receive.